Smart Utility
Smart Utility is designed to make it easier to fill out custom templates, applicable for Constructional, Operational, and Derived parameters. Instead of entering each parameter manually, you can upload an excel file with up to 500 parameters at once. After mapping the data and uploading the file, the best-matched APM parameters are presented for you to accept or modify. You can also adjust the details of each parameter. Once this is done, the parameters automatically appear in their respective sections in the template, and you can continue with the template creation as before.
Accessing Smart Utility
Perform the following steps to access Smart Utility:
-
Navigate to APM Foundation > Template Definition.
-
Click Custom Asset Template > Create Custom Template.
-
Fill in the details in the Template Details section and click Submit.
-
In the Parameter section, click Smart Utility.
Alternatively, you can access Smart Utility by selecting a predefined custom template from the list or clicking the edit icon, and then choosing Parameter > Smart Utility.
The Smart Parameter Mapping page appears with two sections: